How do I configure DDRv tool to connect to a target with other devices present in the JTAG chain?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I configure DDRv tool to connect to a target with other devices present in the JTAG chain?

1,682 Views
tiagobrusamarel
Contributor V

Hello.

 

How do I configure the DDRv tool connection to access a target when other devices are present in the JTAG chain?

 

Regards.

Labels (1)
0 Kudos
Reply
2 Replies

1,552 Views
addiyi
NXP Employee
NXP Employee

For multiple device on chain support in QCVS please contact NXP support.

Adrian

0 Kudos
Reply

1,552 Views
yipingwang
NXP TechSupport
NXP TechSupport

Unlike CodeWarrior, DDRv tool doesn't provide this function.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply