How Node locked license to a dongle license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How Node locked license to a dongle license

2,578件の閲覧回数
jonperez
Contributor I

We have a node locked license. What do we have to do to switch it to a dongle license?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,373件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jon.

Besides Sliva, here is more information.

- I guess your current license should bound with your disk or MAC address. to rehost it to dongle id, you need have a USB dongle anyway. If you don't have it, here you can purchase:

USB Dongle|NXP 

in case you need USB dongle driver, here it is:

USB Dongle Drivers|NXP 

- When you have a USB dongle, you can find the dongle id printed on the dongle, usually it starts with number 9-xxxxxxxx. Please check it.

then you can refer this document to rehost license to USB dongle:

https://community.nxp.com/docs/DOC-103345 

Hope this helps!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,373件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Jon,

Node-locked license could be basicaly locked to MAC address, Disc Volume ID or USB dongle FlexID. If you already have a USB dongle all you need to do is to rehost your license to FlexID printed on your dongle.

Stan

0 件の賞賛
返信