Hello is the CodeWarrior TAP 5V tolerant to be used for the Kinetis KE02 ? Thanks Ad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello is the CodeWarrior TAP 5V tolerant to be used for the Kinetis KE02 ? Thanks Ad

1,056 Views
adgorp
Contributor I

Hello is the CodeWarrior TAP 5V tolerant to be used for the Kinetis KE02 ? Thanks Ad

Labels (1)
0 Kudos
Reply
1 Reply

950 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Ad

CodeWarrior TAP targets for digital networking processors likeQorIQ, StarCore. ..

For details, please refer to:

CodeWarrior TAP|NXP

It does not support Kinetis products. The emulator that supported by CodeWarrior v10.6 for Kinetis includes:

1) P&E Universal Multilink

Universal Multilink Development Interface|NXP

2) P&E Universal Multilink FX

Universal Multilink FX High-Speed Development Inter|NXP

3)  P&E TraceLink

Tracelink - Advance Trace Capture|NXP

4) P&E Cyclone Max

Cyclone MAX|NXP

5) Segger J-Link / J-Trace

SEGGER - The Embedded Experts

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply