Header files of QorlQ P2020

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Header files of QorlQ P2020

1,081 次查看
nareshpuli
Contributor III

hello.. help me,

i want write a GPIO program for QorlQ P2020 processor in ubuntu 

1. please provide me any sample code 

2. what are the headers ?

Regards

Naresh

标签 (1)
0 项奖励
回复
1 回复

945 次查看
Pavel
NXP Employee
NXP Employee

NXP offers Linux SDK v 1.9 for the P2020RDB board:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/qoriq-arm-processors/qori....

 

NXP offers LTIB Linux BSP for the  P2020RDB board:

https://www.nxp.com/webapp/Download?colCode=CWF-ltib_p2020rdb&appType=license&location=null&Parent_n...

 

These BSPs support sysfs possibility for GPIO using under Linux.

https://www.kernel.org/doc/Documentation/gpio/sysfs.txt

http://elinux.org/CI20_GPIO_LED_Blink_Tutorial

 

See also attached file.

 


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复