Freescale HIwave 6.1 in 64-bit Windows 7 Pro

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale HIwave 6.1 in 64-bit Windows 7 Pro

6,201件の閲覧回数
davidschulte
Contributor I

Hello,

 

We are currently trying to migrate our machines to a 64-bit environment.

 

Windows 7Pro 64-Bit

8gb ram

Intel i5 and i7

 

We have no code warrior package but somehow we have Hiwave. Im new to this whole area but I cant seem to find a download of just Hiwave.  I tried downloading the Codewarrior 10.5 Development tools cause I was informed that Hiwave was apart of it.  But when I installed it I was not able to find it.

 

I was able to mimic the setup of hiwave from a 32-bit machine onto a 64-bit machine but the P&E drivers wouldn't work.  That I can point that it came from a 32-bit machine.  So is there a way to make Hiwave 6.1.44 that was on a 32-bit machine work on a 64-bit machine.  Or what Codewarrior package will have hiwave attached to it and will run on 64-bit windows 7 without a problem.

 

We are using HCS08 and MC9S08DN32AMLC

 

 

Thank you

ラベル(1)
0 件の賞賛
返信
1 返信

5,544件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hello David,

CW6.3 includes hiwave debugger.

https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MICROCONTROLLERS

however CW6.3 was not designed for 64bit win7. if you need to work 64bit win7 anyway, please follow below document:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN3936.pdf

=========================================================

this answer is for you, if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 件の賞賛
返信