FreeMASTER crash when configuring Packet Driven BDM communication plug-in

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeMASTER crash when configuring Packet Driven BDM communication plug-in

2,398 Views
daniel_aciubota
Fresh Out Contributor

FreeMASTER crashes when I try to configure the "FreeMASTER Packet Driven BDM Communication" Plug-in.

In the "BDM cable Settings" menu if I click a different option than the default one the program crashes (exits without any message). 

I have this issue using FreeMASTER versions 2.08, 2.09 and 1.4.4 on a system with OS Windows 10 Pro version 1803.

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

2,169 Views
daniel_aciubota
Fresh Out Contributor

The crash was caused by the debugger (P&E Micro) drivers.

An update of the drivers solved the issue.

(The USB Multilink driver version that works is 12.7.0.0 )

2,169 Views
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

in my case it seems to be related to the build of the used Windows 10 version.

Windows 10 Enterprise, Version 1709 works ok but version 1803 doesn't work.

0 Kudos
Reply