Flash Programmer issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Programmer issue

4,813件の閲覧回数
byengsunyang
Contributor II

hi,

board : ls1043ardb , JTAG connection

host :win7-64

codewarrior s/w: evaluation version (QorIQ LS series ARM V8 ISA)

CodeWarrior TAP : network connected

I am having trouble using the Flash Programmer to download u-boot to NOR Flash on the board. "Unprotect" and "erase" of chip are working normally but "programming" does not proceed normally and only "Ignoring packet error, continuing ..." message occurs continuously.
Please give me your feedback on this experience or solution.

Attach a captured screen image.

タグ(2)
0 件の賞賛
返信
5 返答(返信)

4,649件の閲覧回数
addiyi
NXP Employee
NXP Employee

You have to update to the latest version. If you have Compass extranet access you can get the latest CW4NET2017.03. Otherwise, go to Help > Install New Software and select ARMv8 Eclipse Update Site - http://freescale.com/lgfiles/updates/Eclipse/11.2.0/com.freescale.armv8_win as update site.

The first option is strongly recommended.  

Adrian

0 件の賞賛
返信

4,649件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please provide the CW version.

Adrian

0 件の賞賛
返信

4,649件の閲覧回数
byengsunyang
Contributor II

please refer.. version : CW4NET v2016.01

0 件の賞賛
返信

4,649件の閲覧回数
addiyi
NXP Employee
NXP Employee

Go to Help > About CodeWarrior and provide the Version and Build Id.

Adrian

0 件の賞賛
返信

4,649件の閲覧回数
byengsunyang
Contributor II

CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA

(c) Freescale Semiconductor, Inc. 2014. All rights reserved.
Learn more about CodeWarrior at
http://www.freescale.com/codewarrior

Version: 11.2.0
Build Id: 160115

0 件の賞賛
返信