Flash File to Target Problem with Kinetis E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash File to Target Problem with Kinetis E

2,464件の閲覧回数
dhruvonline
Contributor III

Helllo,

 

I have developed a custom KE04Z8- 20pin SOIC based board. I am able to download and debug the program using Main Source Code Project.

But when i use the Flash File to Target option by browsing the Hex File, I am not able to download into the device. It is giving below errors. Please suggest. I am attaching screenshot for the same.

 

Regds,

Dhruv

ラベル(1)
タグ(1)
3 返答(返信)

2,257件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Dhruv ,

In addition, I would like to attach my video for how to use simple flash from my side.

hope this can also help.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,258件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

as noted in the error message of that dialog, you need to specify a target task name.

See that edit box at the bottom of the dialog: specify a name like

MyFlashToFile

or something like this.

I hope this helps,

Erich

0 件の賞賛
返信

2,258件の閲覧回数
dhruvonline
Contributor III

Hi,

Thanks for the response.

I have added the Task Name Also. See the error observed in the second page.

Regds,

Dhruv@ !@New Bitmap Image.bmp

0 件の賞賛
返信