Firmware update required

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware update required

3,814 Views
alikobari
Contributor I

Hello,

I am trying to connect to a target system which is based on p2020 via CW-TAP and using CW- IDE, but I am getting the following error:

 

Error launching Myp2020_project-core00_RAM_P2020_Download

CCSProtocolPlugin : Could not connect to the probe (or other debug link)

[CCS last error: Firmware update required ]

 

11762_11762.pngpastedImage_0.png

 

I did update the firmware by connecting to CW-TAP using ccs.exe in win7 and following command, but I am still getting the same error when I connect to CW-TAP in IDE environment:

 

(bin) 1 % updatecwtap --force 10.92.6.50

10.92.6.50 is running OS version 1.0.1

Update contains OS version 1.0.1

WARNING: Update forced - overriding version check.

WARNING: UPDATING FLASH - DO NOT INTERRUPT!

Sending code to CodeWarrior TAP.........done

Running package script

Erasing kernel partition...

Flashing kernel partition...

Erasing root2 partition...

Flashing root2 partition...

Activating root2

Update completed; rebooting.

Waiting for reboot...

10.92.6.50 is running Boot Loader version 0.9.2

Update contains Boot Loader version 0.9.2

WARNING: Update forced - overriding version check.

WARNING: UPDATING FLASH - DO NOT INTERRUPT!

Sending code to CodeWarrior TAP.........done

Running package script

Erasing uboot partition...

Flashing uboot partition...

Update completed; rebooting.

Waiting for reboot...

All updates completed successfully.

(bin) 2 % updatecwtap 10.92.6.50

10.92.6.50 is running OS version 1.0.1

Update contains OS version 1.0.1

No update needed (use '--force' to reinstall).

10.92.6.50 is running Boot Loader version 0.9.2

Update contains Boot Loader version 0.9.2

No update needed (use '--force' to reinstall).

All updates completed successfully.

(bin) 3 %

 

Thanks

Labels (1)
0 Kudos
Reply
3 Replies

3,053 Views
lunminliang
NXP Employee
NXP Employee

What's your CodeWarrior version? The latest one on CW_DSPA: CodeWarrior Development Studio v10 for Power Architecture® Technology (Eclipse) is 10.3.3 and it supports Windows 7 SP1.

0 Kudos
Reply

3,053 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. CodeWarrior Development Tools or   QorIQ Processors ) to get it visible for active members.

For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )

Thank you for using Freescale Community.

0 Kudos
Reply

3,053 Views
alikobari
Contributor I

Hello Wlodek,

Thank you for your comment, I am new to this community, I will move it right away!

Ali,

0 Kudos
Reply