FS CW JTAG Interface 900-75115 Rev D supported devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS CW JTAG Interface 900-75115 Rev D supported devices

1,612 Views
yandavidov
Contributor I

Hello,

Does the **FreeScale CodeWarrior USB Tap JTAG Interface 900-75115 Rev D COP** support MPC83XX  (MPC8378) processors and flash programming?

can you please list all devices supported with this interface.

Thanks!

0 Kudos
Reply
1 Reply

1,478 Views
alexander_yakov
NXP Employee
NXP Employee

The "900-75115" is not NXP partnumber, correct NXP partnumber should be like this: CWH-UTP-PPCC-HE

The marking "COP" means this is JTAG/COP version of USP tap, it can be used for PowerPC targets (except MPC8xx).

To answer your question - yes, "COP" version of USB TAP supports MPC83xx family processors, including MPC8378, for debugging and flash programming. Note - this debug probe should be used along with CodeWarrior software, for MPC83xx family you should use this version:

CodeWarrior Development Studio for PowerQUICC (Classic IDE) v8.8

CodeWarrior Development Tools for PowerQUICC|NXP 

Link to CodeWarrior USB TAP User Guide:

http://www.nxp.com/assets/documents/data/en/user-guides/CWH-UTP-UG.pdf 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------