ERROR L1115: Function _startup not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ERROR L1115: Function _startup not found

2,100 Views
sagardhavali
Contributor III

Hello All,

 

I am being asked to change the code for a project which as S9S12GA46 MCU. Earlier it was having S9S12GNA16 MCU.

 

Upon modifying the required changes, I am getting above said error. I am attaching the log file here. I hope someone can point me what is that I am missing.

 

Thank You,
Sagar

Original Attachment has been moved to: _makelog.log.zip

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,859 Views
sagardhavali
Contributor III

Problem Fixed.

Apparently, I was supposed to add custom object list to code warrior generated .prm file.

Thank you all.

1,859 Views
sagardhavali
Contributor III

An Update:

I was able to localize the problem. Apparently the problem is with .prm files.
If I use previous MCU's .prm file (mc9s12gna.prm) for new MCU, I don't have any issue. But If I use the correct .prm file (i.e, ms9S12GA48.prm) I get error (Function _Startup not found).

Hoping to find the help.

Thanks

0 Kudos
Reply