Does CYCLONE FX have the function of send result single out?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does CYCLONE FX have the function of send result single out?

1,515 Views
terryli666
Contributor I

Hey guys, I have one question..

      When I used CYCLONE FX to download MCU, I can read  sucess or fail through the LED on it. But if I want to record this result on my computer. Which port should I use for this function? Serial Port? But I can't read the single from it. Does CYCLONE FX have this function to send result single out?If yes, which port should I use?Thanks!

Tags (2)
0 Kudos
Reply
1 Reply

1,246 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Terry,

CYCLONE FX is P&E product but not NXP, Please contact P&E forums or support

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply