Debugger Display Setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugger Display Setting

8,632 次查看
hucklim
Contributor III

Hello all,

I was searching for a way to turn on the symbol hint during debugging. I read from a debugger manual that one

can switch on the symbol hint from the debugger's display setting (edit>preference>debugger...). But my preferences

does not provide the option for the debugger. I am using Codewarrior IDE v5.9.0 build 5294. Is the missing debugger option

to be expected from this version that I am using?

 

Thanks in advance.

 

Yours

Huck

标签 (1)
标记 (1)
5 回复数

8,410 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

what kind of "symbol hint" do you need during debug? can you please upload a screenshot of it? I need to check if CW for HCS12 v5.1 have this feature.

does your CW5.1 never have "symbol hint"? or it ever does ,but doesn't have now?

0 项奖励
回复

8,409 次查看
hucklim
Contributor III

Hello Jennie,

I have found out how to use the ‚Symbol Hint‘ in my debugger. I first need to highlight the parameter and then the value of the parameter does appear. Previously I forgot to highlight the parameter. I just float my

Cursor over the parameter and expected to see the value of the parameter, which is not how it works.

Thanks for your help.

Yours sincerely,

Huck

Von: ZhangJennie

Gesendet: Mittwoch, 25. Dezember 2013 09:45

An: Huck Lim

Betreff: Re: - Debugger Display Setting

<https://community.freescale.com/>

Debugger Display Setting

reply from ZhangJennie<https://community.freescale.com/people/ZhangJennie?et=watches.email.thread> in CodeWarrior Development Tools - View the full discussion<https://community.freescale.com/message/370553?et=watches.email.thread#370553>

0 项奖励
回复

8,409 次查看
hucklim
Contributor III

Hello Jennie,

I installed my codewarrior version 2 weeks ago, I do not know if there is ever ‚symbol hint‘ in this version of my codewarrior. I read from debugger user manual that by placing the cursor over a variable, the value of

the variable should appear. The manual also indicated that one can turn on the ‘symbol hint’ through the ‘Display setting’. However, I could not find the display setting on my codewarrior.

Yours sincerely,

Huck

Von: ZhangJennie

Gesendet: Mittwoch, 25. Dezember 2013 09:45

An: Huck Lim

Betreff: Re: - Debugger Display Setting

<https://community.freescale.com/>

Debugger Display Setting

reply from ZhangJennie<https://community.freescale.com/people/ZhangJennie?et=watches.email.thread> in CodeWarrior Development Tools - View the full discussion<https://community.freescale.com/message/370553?et=watches.email.thread#370553>

0 项奖励
回复

8,409 次查看
TICS_Fiona
NXP Employee
NXP Employee

Could you please reply what is the CodeWarrior version you are using? To get it, please:

1)Start the IDE and click on Help | About Freescale(Metrowerks) CodeWarrior.

2)Click on Installed Products

3)Provide us all info displayed. Or you can save them in a txt file.

8,409 次查看
hucklim
Contributor III

Hello TICS Fiona,

thanks for your reply. The CodeWarrior version that I am using is:

CodeWarrior Development Studio for the S12(X) Version 5.1, build 10221.

I am attaching the Installed Plugins.TXT file so that you can get the information of all the Plugins I am using.

Thanks

Huck

Von: TICS_Fiona

Gesendet: Donnerstag, 19. Dezember 2013 04:17

An: Huck Lim

Betreff: Re: - Debugger Display Setting

<https://community.freescale.com/>

Debugger Display Setting

reply from TICS_Fiona<https://community.freescale.com/people/TICS_Fiona?et=watches.email.thread> in CodeWarrior Development Tools - View the full discussion<https://community.freescale.com/message/369754?et=watches.email.thread#369754>