Debug configuration starts with an error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug configuration starts with an error

ソリューションへジャンプ
17,899件の閲覧回数
janbrand
Contributor II

Hello!

 

I've got a problem with CodeWarrior Development Studio for QorIQ LS series (10.0.8) and my LS1021atwr. I want to use the CodeWarrior TAP for debugging.  I'm not able to open debug configuration without the following Problem: (a jpeg is added to this post, too) "An error has occurred. See error log for more details. com.freescale.sa.configurator.ls.jni.LSConfigLoader_JNI.init(Ljava/lang/String;)V"

I don't know how to fix this...

Had has anyone this error already?

 

kind regards,

Jan

ラベル(1)
1 解決策
17,657件の閲覧回数
addiyi
NXP Employee
NXP Employee

Go to CW_ARMv7/ARMv7/sa_ls/bin and run createlinks_xpcom.sh. Restart CW and try again. This should solved the problem.

Adrian

元の投稿で解決策を見る

16 返答(返信)
17,657件の閲覧回数
addiyi
NXP Employee
NXP Employee

Hi Jan,

Which OS are you using?

Adrian

0 件の賞賛
返信
17,657件の閲覧回数
janbrand
Contributor II

Hi,

actually I'm trying with Ubuntu 14.04 LTS...

Jan

0 件の賞賛
返信
17,657件の閲覧回数
addiyi
NXP Employee
NXP Employee

Did you run setuplinux.sh script and the commands form Dependency installation, in README? This errors is generated by missing of libexpat.

Adrian

0 件の賞賛
返信
17,657件の閲覧回数
janbrand
Contributor II

Yes. First I ran ./setuplinux.sh from the tarball. Then I executed install_deps.sh with root: "~/Freescale/CW4NET_v2016.01$ sudo ./install_deps.sh" and the message: "dependency installed successfully" appears....

Jan

0 件の賞賛
返信
17,657件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please rerun:

1. Ubuntu 12.04/14.04/15.04 or newer

    * Elevate to root using su

    * In the terminal run the following command:

        # sudo apt-get install libc6:i386 libgcc1:i386 gcc-4.6-base:i386 libstdc++5:i386 libstdc++6:i386 libgtk2.0-0:i386 libxpm4:i386 libusb-0.1-4:i386 libusb-1.0-0:i386 libuuid1:i386 libxcb1:i386 libnspr4:i386 libglib2.0-0:i386 libxdamage1:i386 libxtst6:i386 libssl0.9.8:i386

Adrian

0 件の賞賛
返信
17,657件の閲覧回数
janbrand
Contributor II

Hi,

it seems to be all is up to date:

"# sudo apt-get install libc6:i386 libgcc1:i386 gcc-4.6-base:i386 libstdc++5:i386 libstdc++6:i386 libgtk2.0-0:i386 libxpm4:i386 libusb-0.1-4:i386 libusb-1.0-0:i386 libuuid1:i386 libxcb1:i386 libnspr4:i386 libglib2.0-0:i386 libxdamage1:i386 libxtst6:i386 libssl0.9.8:i386Paketlisten werden gelesen... Fertig

Abhängigkeitsbaum wird aufgebaut.      

Statusinformationen werden eingelesen.... Fertig

libusb-0.1-4:i386 ist schon die neueste Version.

libusb-1.0-0:i386 ist schon die neueste Version.

libxcb1:i386 ist schon die neueste Version.

libxdamage1:i386 ist schon die neueste Version.

libxpm4:i386 ist schon die neueste Version.

libxtst6:i386 ist schon die neueste Version.

gcc-4.6-base:i386 ist schon die neueste Version.

libstdc++5:i386 ist schon die neueste Version.

libc6:i386 ist schon die neueste Version.

libgcc1:i386 ist schon die neueste Version.

libglib2.0-0:i386 ist schon die neueste Version.

libgtk2.0-0:i386 ist schon die neueste Version.

libnspr4:i386 ist schon die neueste Version.

libstdc++6:i386 ist schon die neueste Version.

libuuid1:i386 ist schon die neueste Version.

libssl0.9.8:i386 ist schon die neueste Version.

0 aktualisiert, 0 neu installiert, 0 zu entfernen und 44 nicht aktualisiert."

Jan

0 件の賞賛
返信
17,657件の閲覧回数
addiyi
NXP Employee
NXP Employee

Could you please issue next command in your ubuntu terminal "/sbin/ldconfig -vp | grep libexpat" and share the output? Also, could you provide .metadata folder from your workspace?

Adrian

0 件の賞賛
返信
17,657件の閲覧回数
janbrand
Contributor II

Here is the output from /sbin/ldconfig -vp | grep libexpat:

~$ /sbin/ldconfig -vp | grep libexpat

  libexpatw.so.1 (libc6,x86-64) => /usr/lib/x86_64-linux-gnu/libexpatw.so.1

  libexpatw.so.1 (libc6) => /usr/lib/i386-linux-gnu/libexpatw.so.1

  libexpat.so.1 (libc6,x86-64) => /lib/x86_64-linux-gnu/libexpat.so.1

  libexpat.so.1 (libc6) => /lib/i386-linux-gnu/libexpat.so.1

metdata.tar is added to this post...

kind regards

Jan

0 件の賞賛
返信
17,657件の閲覧回数
addiyi
NXP Employee
NXP Employee

The library looks fine. Also, in log I don't see an error related to your first error. Did you still have that error? Did you tried to change the workspace?

Adrian

0 件の賞賛
返信
17,656件の閲覧回数
janbrand
Contributor II

Yes, It's still the same error even if i change the workspace...

0 件の賞賛
返信
17,658件の閲覧回数
addiyi
NXP Employee
NXP Employee

Go to CW_ARMv7/ARMv7/sa_ls/bin and run createlinks_xpcom.sh. Restart CW and try again. This should solved the problem.

Adrian

17,655件の閲覧回数
janbrand
Contributor II

Thank you, that fixed the problem! I can open debug configuration without getting an error.

Now another error comes up (Added a .jpeg to this post). A terminal with ccs starts, but just put something out and closes. I can not get the Output - it's closing too fast... The CodeWarrior TAP is blinkin green on TX/RX (like standard) and for four very short times a red LED is shown. Then CodeWarrior ends with the Error....

Is there a relation between the erros?

kind regards,

Jan

0 件の賞賛
返信
17,655件の閲覧回数
addiyi
NXP Employee
NXP Employee

What is the CPU rev on your board?

Adrian

0 件の賞賛
返信
17,655件の閲覧回数
janbrand
Contributor II

This is what U-Boot is saying:

U-Boot 2014.07+ls1+g6747328 (Dec 07 2014 - 16:03:02)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 70000000 00407900 e0025a00 21046000

       00000020: 00000000 00000000 00000000 00038000

       00000030: 00080000 48007340 00000000 00000000

Board: LS1021ATWR

CPLD:  V2.3

PCBA:  V4.0

VBank: 0

Jan

0 件の賞賛
返信
17,655件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please take a look to LS1021A_TWR_README.txt:

Information about processor revision 1

#--------------------------------------------#

To debug a target with this processor revision you must use the CFG file "LS102xA_Rev1_ConfigChain.cfg" that can be found at the location

[CW install path]/ARMv7/ARM_Support/Configuration_Files/jtag_chains/. This file will be imported following the next steps:

1. Open "Debug Configurations..." and select your project;

2. Click on the "Edit..." button which can be found next to the drop list called "Connection" from the "Target Settings" view;

3. Click on the "Edit..." button which can be found next to the drop list called "Target";

4. Click on the "Edit..." button which can be found next to the drop list called "Target type";

5. Click "Import..." and then "File System..." and select the file specified above and then click OK until you return

to "Hardware or Simulator Target" window;

6. Select in the "Hardware or Simulator Target" window the initialization and memory files from the project;

7. Click OK until you return to "Debug Configurations..." window and click "Debug".

Adrian

0 件の賞賛
返信
17,655件の閲覧回数
janbrand
Contributor II

Ahhh great! That is working too! A big Thank You for your help!

Kind regards

Jan