Debug S12ZVC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug S12ZVC

3,119 Views
thorstenmumm
Contributor III

Hello,

i do now me first projekt with codewarrior and a S12ZVCA, all works fine but i can not youse the debug funktion

i get allways the massage "no source availabel for "0x7E803B ( 0x7E803B0)"

i thing its a problem with configuration the debuger

me work a round ist to send the need Data by can but now i need infos by a Flag and i will set a breakpiont

i have createtd the projekt by Processor expert with a new Bareboard Projekt

how can help?

Thanks Thorsten

Labels (1)
0 Kudos
Reply
5 Replies

2,933 Views
thorstenmumm
Contributor III

now it's works with 10.6 and 10.7!

it was a good idear to youse a exampel.

it was a configbit for the scurity! it must set to disable!

only "NOT initialized" dosent work for debugging

thanks for help!

0 Kudos
Reply

2,933 Views
thorstenmumm
Contributor III

yes, now i try the 10.7 but i get the same error massage

i have the evaluation board for the S12ZVC i think its called HEARTS from 2013 but i find not sampels for it

now i do a other test, i youse my board with an exampel in codewarrior the "LEDBAR" for the ZVC an thats work in debugging! with booth version! 10.6 and 10.7

I think its a problem by the settings but witch?

0 Kudos
Reply

2,933 Views
thorstenmumm
Contributor III

Hi Jennie,

thanks

i try it again, but is the same.

I create a new Projekt without processor expert and i get the same message

I think it works one or tow yaers befor. I dont youse ist in the last time but i change to a new computer and insatll iall new

I use a speziel older version of the codewarrior for the s12ZVC, it was for free and limitit by the space

Version is 10.6.4 Build Id 150416

Thanks

Thorsten

0 Kudos
Reply

2,933 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Did you try CW10.7?

what connection interface do you work with?

the board is a customized board or NXP demo board?

0 Kudos
Reply

2,933 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Thorsten.

There are many reasons causing this problem. The most common reasons is:

1. your CW version is old. you need install update your CW.

2. you didn't select the correct part number.

so please

1. your CW version: Start the IDE and click on Help | About CodeWarrior Development Studio. Send me the version and build id. meanwhile install CW10.7 and try it :

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 

2. then please check your exact chip part number.

then create a NEW project in a NEW workspace WITHOUT processor expert to test it. how does it works?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply