Codewarrier reference applications(Non OS) for MPC8306 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrier reference applications(Non OS) for MPC8306 processor

1,931 Views
nthiru28
Contributor I

Hi All,

 

I'm trying to develop standalone application for MPC8306 based board, which doesn't support any Operating system.

 

Please can anyone suggest me the proper document to start learning about Register Configuration in codewarrior and reference applications except hello world which is default with Codewarrior. ?

 

Regards,

Thiru N

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,813 Views
lunminliang
NXP Employee
NXP Employee

Hello Thiru N,

If you are using CW for PA 10, you could find some bared board example in the CW installation directory:

D:\Freescale\CW_PA_v10.5.1\PA\CodeWarrior_Examples\Bareboard_Examples

If you are using CW for PowerQUICC(Classic IDE), you could also find CodeWarrior example in the CW installation directory:

C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\(CodeWarrior_Examples)

For the "Register Configuration in codewarrior", I am not sure what you mean, please elaorate, thanks.

Regards

Lunmin

0 Kudos
Reply

1,813 Views
nthiru28
Contributor I

Hi Lunmin,

Thanks for your response.

I'm using Code-warrior v8.8 and also using Freescale TAP for programing.

Can you please specify the example application which works for MPC8308

Registry configuration in the sense, the processor initial configuration

and *.lcf file.

Regards,

Thiru N

*For the "Register Configuration in codewarrior", I am not sure what you

mean, please elaorate,*

I'm expecting the configuration file of MPC8308 related to bare code of

On Mon, May 9, 2016 at 10:44 AM, lunminliang <[email protected]>

0 Kudos
Reply