CodeWarrior support for QorIQ T1024 Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior support for QorIQ T1024 Processor

1,490 Views
manjularajesh
Contributor II

We are using CodeWarrior Development Studio for Power Architecture(version 10.3.3, Build Id:131024), Currently we started our design using T1024 processor this Codewarrior version is not supporting T1024RDB. Can we upgrade to higher version for T1024 support?? What is the procedure to upgrade, please provide web-links of the same.

 

regards,

manjula

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,382 Views
trytohelp
NXP Employee
NXP Employee

Hi,

I've checked with the last version CW for PA V10.5.

This version is is supporting the T1024RDB board.

How to get it ?

You can download the tool via our web site:

    CodeWarrior Dev Tools for Power Architecture|Freescale

For the license file, it depends of your registration.

I recommend you to check your registration to see if you can upgrade it for free or not.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply