CodeWarrior for QorIQ LS Series, ARMv8 ISA v11.5.0, where?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for QorIQ LS Series, ARMv8 ISA v11.5.0, where?

3,656 Views
manoloruiz
Contributor III

Where can I get the version "CodeWarrior for QorIQ LS Series, ARMv8 ISA v11.5.0"? I cannot find it anywhere.

0 Kudos
Reply
2 Replies

3,593 Views
Pavel
NXP Employee
NXP Employee

NXP offers the CodeWarrior for QorIQ LS Series ARMv8 ISA. Evaluation / Updates:

https://nxp.flexnetoperations.com/control/frse/product?entitlementId=529066037&lineNum=1&authContact...

Please read the Release Notes associated with the package, describing what is new in this release.

   CW_ARMv8_v2020.06_b200629GA_Linux_Offline.tar

   CW_ARMv8_v2020.06_b200629GA_Linux.tar

   CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe

   CW_ARMv8_v2020.06_b200629GA_Win_Setup.exe

   CodeWarrior_ARMv8_v11_5_0_Release_Notes.pdf

The files are available for download in your Software Account.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,593 Views
manoloruiz
Contributor III

I guess it is inside CW4NET_v2020.06 but I cannot find it anywhere

0 Kudos
Reply