CodeWarrior for QorIQ LS Series, ARMv8 ISA v11.5.0, where?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for QorIQ LS Series, ARMv8 ISA v11.5.0, where?

3,665件の閲覧回数
manoloruiz
Contributor III

Where can I get the version "CodeWarrior for QorIQ LS Series, ARMv8 ISA v11.5.0"? I cannot find it anywhere.

0 件の賞賛
返信
2 返答(返信)

3,602件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers the CodeWarrior for QorIQ LS Series ARMv8 ISA. Evaluation / Updates:

https://nxp.flexnetoperations.com/control/frse/product?entitlementId=529066037&lineNum=1&authContact...

Please read the Release Notes associated with the package, describing what is new in this release.

   CW_ARMv8_v2020.06_b200629GA_Linux_Offline.tar

   CW_ARMv8_v2020.06_b200629GA_Linux.tar

   CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe

   CW_ARMv8_v2020.06_b200629GA_Win_Setup.exe

   CodeWarrior_ARMv8_v11_5_0_Release_Notes.pdf

The files are available for download in your Software Account.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,602件の閲覧回数
manoloruiz
Contributor III

I guess it is inside CW4NET_v2020.06 but I cannot find it anywhere

0 件の賞賛
返信