CodeWarrior 10.3 with MPC5643L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 10.3 with MPC5643L

2,538 Views
DC08
Contributor I

Hey Guys,

 

I'm new to CodeWarrior and the Power PC Architecture and I'm trying to get a simple example running on the MPC5643L using CodeWarrior 10.3. I'm using the PXC56XL 144LQFP Mini-Module along with the EVB Motherboard that goes along with it. Does anyone have an example project they can send me that is running at least the LEDs on the Motherboard? I haven't been able to find any working project. I was able to find one project, but when I compile it, I get the following error:


mingw32-make: *** Error 1


Does anyone know how to get rid of this? Thank you.

Labels (1)
0 Kudos
Reply
2 Replies

2,311 Views
TICS_Fiona
NXP Employee
NXP Employee

CW10.3 has include an exmaple for MPC5643L:
C:\Freescale\CW MCU v10.3\MCU\CodeWarrior_Examples\Qorivva_Examples\MPC5643L_INTC-SW-VLE-LSM

0 Kudos
Reply

2,311 Views
DC08
Contributor I

I found it easiest to download CodeWarrior v10.5 and install the Qorivva Support. I tried looking for the examples through there but I found nothing. its because I had CW for Power Architecture v10.3. Once I downloaded the Qorivva support on v10.5 I was able to get an example project created and continue on from there.

0 Kudos
Reply