CodeWarrier Support in linux unix

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrier Support in linux unix

1,550件の閲覧回数
deekshithachary
Contributor I

Hi,

We are using Codewarrier version CW_SC_v10.6.4. We wanted to know whether there is any support for Codewarrier compiler available for UNIX/LINUX.?

 

Thanks and Regards,

Deekshith Acharya

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,419件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Deekshith,

We've 2 product families for CodeWarrior:

     - CodeWarrior Development Suites for Networked Applications (CW4NET),

     - CodeWarrior development Suites (Basic, Standard and Professional).

The Development tools for StarCore devices are available under  CW4NET.

There are 3 versions:

     CodeWarrior for StarCore 3900FP DSP Eclipse V10.9.0

     CodeWarrior for StarCore 3850 Eclipse Evaluation / Updates V10.7.2

     CodeWarrior for Starcore DSP, Windows WIN Evaluation / Updates V3.2

For V10.9.0 we've  Windows and Linux versions.

     CodeWarrior Dev Tools for StarCore 3900FP DSP|NXP

For V10.7. and V3.2 windows version is available only.

Regards

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,419件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Deekshith,

Which MCU are you using?

The last CodeWarrior version supported in Linux was CodeWarrior 10.2, it can be downloaded from the following page and it supports Ubuntu 10.04:

CodeWarrior Legacy Downloads|NXP

Click on "Evaluation: CodeWarrior for MCU 10.2 Eval (Linux)"

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信