Code Warrior Burning new U-boot Execute command is not enabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior Burning new U-boot Execute command is not enabled

ソリューションへジャンプ
5,484件の閲覧回数
yusufalti4444
Contributor I

Hi NXP,

I am trying to burn new U-boot on T1042 D4 RDB as described in QorIQ SDK V2.0 - 1703 (Chapter 5) using Code Warrior for T1042. It's the latest Code Warrior Development Studio. I created a sample BareBoard project for T1042 D4 RDB. 

I created a new Target Task as described in documentation but Execute command on Target Task window is not getting enabled. I can run project and I am having console logs.  Documentation says it gets enabled when the debugger is online. My Code Warrior Tab is working. TX/RX led is blinking green and RUN/PAUSE led is lighting red.

I attached Screenshots for more information. Console logs and disabled Execute button can be seen in these screenshots.

What is the reason of this situation, how can I solve it ?

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
5,387件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ahmet Demir,

For flash programming, please refer to the step by step document Flash Programmer for CodeWarrior Power Architecture

1. First please create a board project with Download/Connect SRAM launch configuration.

2. Please import XML task template file for T1042D4 RDB, and add flash programing action in "PA Flash Programmer Task". .

3. Please connect to the target board from Run->Debug configuration -><project>-core00_SRAM_T1040_Connect->Debug, then the "Execute" button is available.

4. Please click "Execute" button to perform flash programming.

Thanks,

Yiping

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
5,388件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ahmet Demir,

For flash programming, please refer to the step by step document Flash Programmer for CodeWarrior Power Architecture

1. First please create a board project with Download/Connect SRAM launch configuration.

2. Please import XML task template file for T1042D4 RDB, and add flash programing action in "PA Flash Programmer Task". .

3. Please connect to the target board from Run->Debug configuration -><project>-core00_SRAM_T1040_Connect->Debug, then the "Execute" button is available.

4. Please click "Execute" button to perform flash programming.

Thanks,

Yiping

 

0 件の賞賛
返信