CW for MCU V10.6.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW for MCU V10.6.4

1,933 Views
danielchampagne
Contributor II

I have downloaded CW for MCU V10.6.4.  It works fine but I just realized that I downloaded the wrong edition.  I downloaded the evaluation edition (which expires in 30 days).  Can someone direct me to the free edition (which has a code size restriction)?

 

 

Thank you

Daniel Champagne

Labels (1)
2 Replies

1,593 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Daniel,

There is no need to reinstall a different CodeWarrior version, the Professional Evaluation Edition you downloaded will start working as a Special Edition (free, permanent, but feature limited) after the 30 days of evaluation ends.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,593 Views
danielchampagne
Contributor II

Thank you! Saves me installing a new version.