CW for MCU 10.6/10.6.4 SE (Eclipse) Licensing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW for MCU 10.6/10.6.4 SE (Eclipse) Licensing

2,707件の閲覧回数
sergiomadrigal
Contributor II

Hi NXP Technical Support

I am currently working with the FRDM-KL25Z hardware and I am going to use CW for MCU 10.6 SE (Eclipse) to programming. I would like to know, Does this license perpetual or only work for 30 evaluation days? and Does it enterprise or academy license? Is it the same way for CW for MCU 10.6.4 SE (Eclipse)?

 

Regards.

 

Sergio

5 返答(返信)

2,435件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Sergio,

you use CW for MCU 10.6.4 SE, here "SE" means special edition.

special edition  is a perpetual version, but it has code size limit:

Kinetis E, L, M Series: 64 KB
Kinetis K Series: 128 K

If you work with evaluation version. there is no code size limit, but has 30 days time limit.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,435件の閲覧回数
sergiomadrigal
Contributor II

Hello Jennie,

I have one question more. You said that this is a perpetual version. However perpetual not always means free, so Has the CW 10.6.4/10.6 SE  free and enterprise license?

Kind regards

Sergio

0 件の賞賛
返信

2,435件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Sergio

CW 10.6.4/10.6 SE  is free and perpetual. But it has code size limit.

In fact, CW 10.6.4/10.6 executes special edition in default level.  That’s to say, even there is no license installed under CW, it is SE  is free and perpetual. But it has code size limit. If your project C code size is under this limit, you can use it for your project for free.

Kinetis E, L, M Series: 64 KB
Kinetis K Series: 128 K


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,435件の閲覧回数
sergiomadrigal
Contributor II

Hello Jennie

Thanks a lot!

Regards

Sergio

0 件の賞賛
返信

2,435件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome.

Have a great day,
Jennie Zhang

0 件の賞賛
返信