CW for MCU 10.6/10.6.4 SE (Eclipse) Licensing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW for MCU 10.6/10.6.4 SE (Eclipse) Licensing

2,731 Views
sergiomadrigal
Contributor II

Hi NXP Technical Support

I am currently working with the FRDM-KL25Z hardware and I am going to use CW for MCU 10.6 SE (Eclipse) to programming. I would like to know, Does this license perpetual or only work for 30 evaluation days? and Does it enterprise or academy license? Is it the same way for CW for MCU 10.6.4 SE (Eclipse)?

 

Regards.

 

Sergio

5 Replies

2,459 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Sergio,

you use CW for MCU 10.6.4 SE, here "SE" means special edition.

special edition  is a perpetual version, but it has code size limit:

Kinetis E, L, M Series: 64 KB
Kinetis K Series: 128 K

If you work with evaluation version. there is no code size limit, but has 30 days time limit.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,459 Views
sergiomadrigal
Contributor II

Hello Jennie,

I have one question more. You said that this is a perpetual version. However perpetual not always means free, so Has the CW 10.6.4/10.6 SE  free and enterprise license?

Kind regards

Sergio

0 Kudos
Reply

2,459 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Sergio

CW 10.6.4/10.6 SE  is free and perpetual. But it has code size limit.

In fact, CW 10.6.4/10.6 executes special edition in default level.  That’s to say, even there is no license installed under CW, it is SE  is free and perpetual. But it has code size limit. If your project C code size is under this limit, you can use it for your project for free.

Kinetis E, L, M Series: 64 KB
Kinetis K Series: 128 K


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,459 Views
sergiomadrigal
Contributor II

Hello Jennie

Thanks a lot!

Regards

Sergio

0 Kudos
Reply

2,459 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome.

Have a great day,
Jennie Zhang

0 Kudos
Reply