CW 10.6 special edition suddenly shut down after 2 sec (Win7-64)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.6 special edition suddenly shut down after 2 sec (Win7-64)

3,349 Views
oliverrichter
Contributor I

Hi together

I had the problem now on 3 different win7-64 PC's:

I start Codewarrior (Special Edition for Kinetis, V 10.6).

After about 2 seconds, it disappears.

 

I used this CW version since it was released, and it worked on all 3 PC's before.

I usually change a lot on PC's, as developer, try new software, new hardware, install / update drivers etc. etc.

It is difficult to figure the reasoun out by stepping back to a previous state of PC, repeat all

changes, etc. etc. This is just too much effort.

 

I tried a lot: Re-Installing, updating, downgrading, registry clean, malware check, etc. etc.

Only thing which worked was setting a previous restore point on win7.

But this is not a permament solution, as the problem ocurs again and again, and after restoring,

win7 has "new updates", after which the problem re-occurs.

 

I can't analyze this or figure out the reason.

 

Any help would be appreciated.

Labels (1)
0 Kudos
Reply
7 Replies

3,184 Views
BlackNight
NXP Employee
NXP Employee

Hi Oliver,

can you check (or share) the .log file in of your workspace (it is inside the .metadata folder of the workspace).

This is an Eclipse text file and contains a debug log, maybe it shows the problem?

Erich

0 Kudos
Reply

3,184 Views
oliverrichter
Contributor I

Here is the workspace/.metadata/.log - file from the PC where the version is broken:

!SESSION 2015-01-21 15:07:18.320 -----------------------------------------------

eclipse.buildId=I20070613-1755

java.version=1.6.0_15

java.vendor=Sun Microsystems Inc.

BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en

Command-line arguments:  -os win32 -ws win32 -arch x86

!ENTRY org.eclipse.osgi 2 1 2015-01-21 15:07:21.658

!MESSAGE NLS missing message: ContentTypes_errorDialogAlreadyExists in: org.eclipse.ui.internal.messages

!ENTRY com.freescale.core.ide.cdt.toolchain 4 0 2015-01-21 15:07:27.664

!MESSAGE Environment Variable Dependency not resolved for 'ARMGNUDirEnv'.

!ENTRY com.freescale.core.ide.cdt.toolchain 4 0 2015-01-21 15:07:27.664

!MESSAGE Environment Variable Dependency not resolved for 'ARMSummonDirEnv'.

!ENTRY com.freescale.core.ide.cdt.toolchain 4 0 2015-01-21 15:07:27.664

!MESSAGE Environment Variable Dependency not resolved for 'ARMYagartoDirEnv'.

!ENTRY com.freescale.core.ide.cdt.toolchain 4 0 2015-01-21 15:07:27.664

!MESSAGE Environment Variable Dependency not resolved for 'ARMdevkitProDirEnv'.

!ENTRY com.freescale.processorexpert.core 1 0 2015-01-21 15:07:27.695

!MESSAGE Plugin com.freescale.processorexpert.core.service ProcessorExpertServiceProvider

!ENTRY com.freescale.core.ide.wizard.ui 2 0 2015-01-21 15:07:30.379

!MESSAGE External elements location 'C:\Freescale\CW MCU v10.6\eclipse\../MCU/lib/wizard_data/mqx/4.0/ppc' does not exist

!ENTRY com.freescale.core.ide.wizard.ui 2 0 2015-01-21 15:07:30.379

!MESSAGE External elements location 'C:\Freescale\CW MCU v10.6\eclipse\../MCU/lib/wizard_data/mqx/4.0/patches' does not exist

!ENTRY com.freescale.core.ide.wizard.ui 2 0 2015-01-21 15:07:30.566

!MESSAGE External elements location 'C:\Freescale\CW MCU v10.6\eclipse\../MCU/lib/wizard_data/mqx/4.1/ppc' does not exist

!ENTRY com.freescale.core.ide.wizard.ui 2 0 2015-01-21 15:07:30.566

!MESSAGE External elements location 'C:\Freescale\CW MCU v10.6\eclipse\../MCU/lib/wizard_data/mqx/4.1/patches' does not exist

0 Kudos
Reply

3,184 Views
BlackNight
NXP Employee
NXP Employee

Unfortunately, that log does not show the problem.

0 Kudos
Reply

3,184 Views
oliverrichter
Contributor I

Indeed, unfortunately not :-(

0 Kudos
Reply

3,184 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Oliver,

Do you solve your problem as I tell you on "Freescale CRM" ?

like this :

" Please right click on the desktop, then select personalize , enter the "Aero Themes", select the basic themes "Windows 7"."

BR

Alice

0 Kudos
Reply

3,184 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Oliver,

1)Does the 3 pc all can't run the CW10.6 now ?

2) And does when start cw, do nothing ,it closed?   If not , when it can't work ?

3) Please screenshot your CW version and build ID like this

pastedImage_0.png

pastedImage_1.png

BR

Alice

0 Kudos
Reply

3,184 Views
oliverrichter
Contributor I

Seems to be the same version, only the listed plugins are slightly different.

codewarrior_about.jpg

0 Kudos
Reply