Hi Support staff; Is there a fix to this coming, or done?
e are trying to manage many projects and the list is out of control, makes it really hard to understand what is what across multiple projects.
Hi Carl,
I'm remember I met the problem in the past too.
I've tried to reproduce it with the MCU v10.6 with a sample project.
However it seems it's working fine.
The CW_MCU_v10_6_Update_3_0_0 was released last month.
This Update solved a problem with Target Task:
* ENGR00330546 - Flash actions settings lost after close then re-open a target task.
This is may be linked to the problem you reported.
Can you try to install the last patches ?
Perform a Help + Check for Updates and Help + Install New Software...
Attached the release notes
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Pascal,
I am having this problem also. I am running CW 10.6.4 Update 6, which is the latest available. So it appears that either the problem came back, or that update did not actually fix the problem.
Thanks.
Problem is I cant update CW10.6, when I try I get this dialogue box (help > check for updates > agree to licnese > it downloads for a while then >
An error occurred while collecting items to be installed
session context was:(profile=PlatformProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Problems downloading artifact: binary,com.freescale.mcu10_6.update_root,3.0.0.
MD5 hash is not as expected. Expected: 78908cbc73bdce58824b3e8ef37be5d2 and found 8015c2223eaff5797d8631c5401fc5aa.
Just another typical experince with CW.
How do I update from here?
well I just selected the 3.0.0 updates from the massive list of updates and that worked, after the restart I installed the rest of hte updates and got:
An error occurred while collecting items to be installed
session context was:(profile=PlatformProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/MCU10_6/com.freescale.mcu.updatesite/plugins/com.freesc....
chunked stream ended unexpectedly
If i try some other updates only:
An internal error occurred during: "Updating Software".
Profile PlatformProfile is not current. Expected timestamp 1424993238977 but was 1424993222043.
so glad we pay a yearly subscription for something that I spend more time fighting than using.
And another, this is for processor expert for MCU 10.6.3.RT6_b1146-0504
An error occurred while collecting items to be installed
session context was:(profile=PlatformProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/MCU10_6/com.freescale.mcu.updatesite/plugins/com.freesc....
chunked stream ended unexpectedly
I played this game where you guess what order things need to be installed in and what dependencies they have, finally beat it, would play again, 5 stars. Would be a boring game if someone automated this process.
Hello Carl,
Sorry for the delay.
To avoid confusion I will create a new post for your question.
The fist time I've checked the issue I was pretty sure it was already handle.
Refer to CW 10.6 is duplicating a target task every time CW is initialized. How to get rid of this? for details.
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------