CMSIS lib with MQX Lite RTOS ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS lib with MQX Lite RTOS ?

3,849件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hi

I am using K60 uc with codewarrior 10.6. currently, I want to interface CMSIS library with MQX_Lite RTOS. I have build the library and tested it on codes without RTOS for K60. It is working fine but as I tried interfacing it on the MQX_Lite RTOS it started showing errors. These error came only by including arm.math.h which is the standard header file used in all the program using CMSIS lib. I tried including it in main.c or  mqx_task.c but in both cases this error was there.

 

14108_14108.jpgcmsis2.jpg

 

14109_14109.jpgCMSIS.jpg

 

Please look into the matter and help me to resolve this issue. Attached is the build library along with the code.

 

Kind regards

Amit Kumar

Original Attachment has been moved to: CMSIS_4.0.1.zip

Original Attachment has been moved to: K60-MQX-CMSIStest.zip

ラベル(1)
タグ(5)
6 返答(返信)

3,384件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Amit, please refer http://mcuoneclipse.com/2013/02/14/tutorial-using-the-arm-cmsis-library/ to manage your code. please make sure all the source code paths are included in project settings. ZhangJun

0 件の賞賛
返信

3,384件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hi Zhang

Thanks for reply. I have been through that tutorial and have successfully implemented it with baremetal code. I am facing issue in implementing with MQX light RTOS.

Kind Regards

Amit Kumar

0 件の賞賛
返信

3,384件の閲覧回数
menkooldewurtel
Contributor II

Hi Amit,

I also have this problem with the same errors. I have the CMSIS library as it says in the tutorial included, without MQX Lite everything works.

Have you solved the problem?

Thank you for your answer

Menko Oldewurtel

0 件の賞賛
返信

3,384件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hi Menko

The Issue is still not resolved.

Regards

Amit

0 件の賞賛
返信

3,384件の閲覧回数
menkooldewurtel
Contributor II


Hi Amit,

i tried with KDS version 2.0. There are no errors like in CW.

Regards

Menko

3,384件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hi Menko

Thats good to know. Its working properly?

Regards

Amit

0 件の賞賛
返信