CDC Example on MC9s08jm60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CDC Example on MC9s08jm60

1,382 Views
elettronicarewo
Contributor I

Hi, I'd like to try the CDC class example (find in USB STACK).I never  use USB and this micro before, so i have a dubt: which XTAL i need to use for run the example as is it? Can i use 4MHz? Anyone can help me to calc the value for set proprery the register?

Labels (1)
0 Kudos
Reply
1 Reply

1,318 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

regarding the CDC demo code for MC9S08JM60, please use below USB stack v4.1.1:

USB Stack v4.1.1 Freescale bare metal (no OS) USB Stack

Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply