Automotive Math and Control Functions in Freescale CodeWarrior Classic IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Automotive Math and Control Functions in Freescale CodeWarrior Classic IDE

1,645 Views
dynexdave
Contributor II

I'm trying to use Automotive Math and Control Functions in Freescale CodeWarrior Classic IDE. I have the dual PMSM development kit and I'm trying to build a project as a staring point based on the c code provided with the kit.   The code uses functions from the Automotive and Motor control library, which I've downloaded, but I can't work out how to tell my project where these files are. When trying to add all header files manually I get a warning saying some files couldn't be added. CodeWarrior Newbie :smileyhappy:

0 Kudos
Reply
1 Reply

1,554 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi David,

To investigate the problem, we need more information.

1. your CW version.

2. which “Automotive and Motor control library” do you work with? please send me the link thus I can check it .

Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply