Any major differences between CW USB TAP and CW TAP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Any major differences between CW USB TAP and CW TAP?

2,335件の閲覧回数
mariochan
Contributor I

Hi Tech support,

 

I previously purchased CW USB TAP.

 

Probe Tip:  Power Architecture JTAG/COP

PC window 7 64 bit.

PC installed Power Architecture 8.8

 

Target PCB with the processor: MPC8358ECVRAGDGA

 

It worked. Typed "findcc utaps" @ CCS, it shows my CW USB TAP serial number.

I am able to "erase" in flash programmer.

 

Problem:

I purchased CW TAP (Supports USB and Ethernet)  for mass production.

PC window 7 64 bit. (Same)

PC installed Power Architecture 8.8 (Same)

 

Target PCB with the processor: MPC8358ECVRAGDGA (Same)

 

It failed. Typed "findcc utaps" or "findcc ethaps", etc @ CCS. It does not show anything.

I am NOT able to "erase" in flash programmer, it shows check JTAG clock speed.

 

 

i have set netparam as following:

 

core> netparam

ethernet_address        = 00:04:9F:03:9B:ED

bootconfig              = static:FSL039BED

static_ip_address       = 169.254.3.4

static_dns_server       = <none>

static_hosts            = <none>

static_routes           = <none>

 

 

PC directly connects to CW TAP.

PC's ip= 169.254.3.2

PC's subnet mask= 255.255.0.0

 

 

Please advise.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,122件の閲覧回数
addiyi
NXP Employee
NXP Employee

The correct command for finding cwtap in ccs is: findcc cwtaps. Because you are using an old version of CW, it is possible that your ccs version to not support cwtap. Here is a document showing how to update ccs for cwtap usage (it is  not for your version of CW, but is applicable).

Adrian

0 件の賞賛
返信

2,122件の閲覧回数
mariochan
Contributor I

Hi Adrian,

Which version should i use for supporting cwtap?

Current version is Power Architecture 8.8.

My company also has version Power Architecture 10.0.2. Does it support cwtap?

If not, which version should i get?

Thanks for the support.

Mario

0 件の賞賛
返信

2,122件の閲覧回数
addiyi
NXP Employee
NXP Employee

Hi Mario,

The latest version of CodeWarrior is 10.5, and this is the version recommended. But, you can follow the steps from the doc, and use a version of ccs that supports cwtap in your CW 8.8 version.

Also, you can check if your PA 10.0.2 supports cwtap, by opening ccs and probe the command: findcc cwtaps.

Adrian

0 件の賞賛
返信