Adding user defined code for FlexRay Code Example for MC9S12XF512.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding user defined code for FlexRay Code Example for MC9S12XF512.

1,629 Views
shanbh01
Contributor I

Could someone on how to edit Flexray sample code with user defined functions and compile successfully ?

I tried by adding a simple user defined function (which writes to console ). It does not seem to work.

I have also included the required headers.

I get few warning indicating "Functional call return value is ignored"

Any sort of help is welcomed. I am really stuck.

Setup:-

Code warrior Dev studio V5.9

Windows OS

Sample code trying to edit: EVB9S12XF512E

Regards,

Rakshith Shnabhag

0 Kudos
Reply
1 Reply

1,560 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Rakshith,

According to your second request in salesforce, you are trying to use fopen and fprintf.

A similar question was discussed in this thread.

Write in a  file in Codewarrior 

Best Regards,

Diana

0 Kudos
Reply