ARM7 Compile using Codewarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ARM7 Compile using Codewarrior

1,803 次查看
bsd9109
Contributor I

hello

My Company name is YURA CORPERATION.

I'd like to compile this project through the Codewarrior.

I'm using the ARM7 mcu in the making STMicroelectronics.

Could you explain why this error happen and i'd like to resolve this error.

thank you.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,749 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Sang,

Now CodeWarrior doesn't support 3rd party MCU. It only supports our own product.

Which version of CW do you work with?


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复