signal when debugger crashes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

signal when debugger crashes

2,522件の閲覧回数
mel
Contributor I

The debugger seems to crash randomly.

If it crashes while I have a motor in boost it burns out the board.

Is there a signal from the processor that will let me know when the debugger

crashes? I am using codewarrior 7.3 on the 56f8357.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,108件の閲覧回数
Oppie
Contributor I
Let me expand on this.
There are some high power processes under control of the processor. When emulation stops, we need a graceful way to shut down the power processes so that the board does not burn up.
 
Is there some hardware method to flag when emulation stops on a breakpoint or emulation failure?
 
codewarrior 7.3 on the 56f8357.   Emulating through the parallel port using OCDemon 'wiggler' jtag converter.
 
TIA
0 件の賞賛
返信