sdm and idm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sdm and idm

2,567件の閲覧回数
siri
Contributor I
hello,

what is the difference between the sdm and idm CPU configuration ? and as well as xROM and pROM.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,301件の閲覧回数
trytohelp
NXP Employee
NXP Employee
duplicated question:
 
sdm: small memory
ldm: large memory
 
For DSP there are 2 memories: DATA and CODE
DATA  is defined by x
CODE is defined by p
For each memory there are:
 External, flash, ram and for DATA IO.
So by this way xRAM is the RAM from DATA and pRAM is the RAM from CODE
 
for details I recommend you to create a project with Processor Expert.
Under Processor Expert menu you can open the Memory Map.
Some information is given in the cmd file too.
 
Hope this will help you.
Pascal
0 件の賞賛
返信