request_irq library in CodeWarrior for ColdFire Linux v2.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

request_irq library in CodeWarrior for ColdFire Linux v2.5

2,118 Views
Bastaix
Contributor I

Where can I get the "request_irq" and "free_irq" functions library for "CodeWarrior for ColdFire Linux v2.5"

 

I need to communicate to RS484 port and I have to reply in less than 1 ms after message read from port to avoid bus colistions.

 

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,037 Views
fsl_linux_spt
Contributor III

I believe that request_irq and free_irq are provided by the kernel, and it should be done from a kernel module and not a userland application.

 

http://www.linuxjournal.com/article/6946

 

http://**bleep**.grm.hia.no/dat2311/man/man9/request_irq.html

 

 

0 Kudos
Reply