problems with freemaster

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

problems with freemaster

2,617 次查看
lijiacui
Contributor I

hello!

I want to use SPI to receive datas from the sensor and hope to  show data on PC by PC_Master. Does the project work?

 

I debug the example for PC_Master 56F8357,it works.But the same program on 56F8346 does not work and does not generate the pmp files,why?

 

Thank you very much!

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,457 次查看
lijiacui
Contributor I

The program used on 56F8346 can make and debug ,but can not generate the pmp files .why? thank your answer ,Tom!

0 项奖励
回复

1,457 次查看
lijiacui
Contributor I
Is there anyone who can help me?
Thank you!
0 项奖励
回复

1,457 次查看
J2MEJediMaster
Specialist I

There's not much detail to "it does not work" to go on here. Are you using the exact same code for the 56F8346 that you used on the 56F8357? There are probably enough differences between the two processors (certain I/O pins, or a different clock frequency) so that the code does not work.

 

---Tom

0 项奖励
回复