internal error 2753. dpinst.exe 1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

internal error 2753. dpinst.exe 1

3,290件の閲覧回数
pnswdv
Contributor I

I have been tasked with supporting some legacy code.  I attempted to install CodeWarrior Development Studio for S12(X) 5.1, which partially completed and then displayed an error dialog "internal error 2753. dpinst.exe 1".  After closing the dialog the installation seemed to complete but the installation is non-functional.  When I try to uninstall the behavior is the same : the uninstall seems to proceed normally but then the error dialog is displayed.

Note: I already had a licensed version of the PEmicro apps and drivers installed before attempting to install CodeWarrior, and they continue to work OK so those drivers seem OK.

Thanks for your help.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,712件の閲覧回数
pnswdv
Contributor I

Thanks Alice,

The PC exceeds the requirements you posted.

Running the installer as administrator did not fix the problem

0 件の賞賛
返信

2,712件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Paul,

Does your CW can work well now ?

If still can't , you can change to another PC, then compare the difference between two PCs.

Please download it in NXP website , also you can use the latest version CW v5.2 .

BR

ALice

0 件の賞賛
返信

2,712件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Paul,

1. What about your PC system ?pastedImage_1.png

2. Please use the Windows admin right to install and open CW.

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信