i have problem for 56800/e flash programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i have problem for 56800/e flash programmer

2,081 Views
chang-hwanshim
Contributor I

hi~ every one~

i have a project that i try to read the memory in 56F803(digital signal controller) by 56800/e flash programmer.

but i can't not read the memory. however progremmer give me the message.

message: Could not write to the Program-RAM, this sally means the wrong configuration file was used.

but i checked configuration file over and over~ 56f803x_.cfg file used~ and i use hardware USBTAP

could you advice something about this problem?

have good time~

0 Kudos
Reply
1 Reply

1,418 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Chang,

56800E Flash Programmer only works for 56800E, and it doesn't not support 56800 product.

To program DSP56F803, please use CodeWarrior, or flash_over_jtag.

CodeWarrior v8.3 can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

It supports programming with USBTAP and Parallel. 

flash_over_jtag is a command-line tool, however it does not support USBTAP. 

Hope it helps! If not, please contact me again. I will be very glad to help you.

Regards,

0 Kudos
Reply