block select

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

block select

1,569 Views
barbercolman
Contributor III

New to CW10  and I am looking for the block select. I can select a number of lines but not a block of text.

 

I want to be able to copy and past the block of text that contains just the the nine ys.

xxxyyyxxx

xxxyyyxxx

xxxyyyxxx

 

 

 

Thanks

Labels (1)
0 Kudos
Reply
2 Replies

1,250 Views
J2MEJediMaster
Specialist I

I did an on-line search and that feature was broken in Eclipse and in a bug report. The traffic that mentioned this was dated 2005. I didn't see where it had been fixed, but I could be wrong on this.

 

---Tom

0 Kudos
Reply

1,250 Views
irob
Contributor V

Same here.  Just installed 10 and "playing" with it.  No block select that I can find.  Are you kidding me?  This is a code editor and no block select?  Good grief, that's embarrassing.

0 Kudos
Reply