Windows XP Professional Service Pack 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows XP Professional Service Pack 2

6,531 Views
rickd
Contributor I
Are there any known issues with Microsoft Windows XP Professioal with SP2?  Have installed CodeWarrior IDE ver. 5.7.1856 with connection to SC140e Platform 2002.  CW launches but application is slow, hangs in servial editor windows.  Other desktops with SP1 running same version of CW do not have this problem.
Thanks,
Rick
Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

2,325 Views
CrasyCat
Specialist III

Hello

may be a FLEXlm issue.

Can you check if environment variable LM_LICENSE_FILE is defined on your system (just open a DOS window and enter the command set LM_LICENSE to get that).

Is that environment variable defined? How is it initialized?

CrasyCat

0 Kudos
Reply

2,325 Views
rickd
Contributor I

Thanks for the reply!

I get the following:

C:\>set LM_LICENSE
LM_LICENSE_FILE=D:\Modeltech_xe_starter\win32xoem\licens
7789@slictx30-002;7789@sigi;7571@slictx30-001;7572@phydo
erks\CodeWarrior for StarCore And SDMA 1.0\license.dat

0 Kudos
Reply

2,325 Views
CrasyCat
Specialist III

Hello

Here CodeWarrior is going to the web to search for license info :smileysad:.

Try placing the local directories before the remote one.

make sure the {...}Metrowerks\CodeWarrior for StarCore And SDMA 1.0\license.dat comes before the 7789@... stuff.

This should go faster.

CrasyCat

0 Kudos
Reply

2,325 Views
rickd
Contributor I

Thanks!!!

That resolved the 'hang-ups'...

0 Kudos
Reply