When Will CodeWarrior Run On Windows Vista?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When Will CodeWarrior Run On Windows Vista?

38,893 次查看
FC
Contributor III
Hello,
 
Will there be a patch for CodeWarrior to run on Windows Vista soon?  All new computers come with Vista, I need to upgrade my computer which runs Windows 98SE because CodeWarrior runs very slow on this computer.
 
Thanks
标签 (1)
0 项奖励
回复
48 回复数

7,209 次查看
CrasyCat
Specialist III
Hello
 
Which processor are you targeting?
I know we should have soon a version of CodeWarrior running on Vista for HC(S)08/RS08.
 
CrasyCat
0 项奖励
回复

7,209 次查看
Andrey
Contributor III
And how soon is that? My company just ordered new laptop for me and it has Vista on it. By the way, I'm still waiting for the Windows XP 64-bit addition of the driver, for my workstation! I cannot program the MCU with it either.
0 项奖励
回复

7,209 次查看
CrasyCat
Specialist III
Hello
 
I have checked with marketing.
Launch Date for CodeWarrior for MCU V6.0 is planned for end of this month (around June 26th).
 
CrasyCat
0 项奖励
回复

7,209 次查看
HansenOnDk
Contributor I
Hello,
 
Just want to follow this topic as seems to be we have already middle of July.
 
Regards,
Tadek, first time on boards..
0 项奖励
回复

7,209 次查看
Alban
Senior Contributor II
Hello,

Yes, I can confirm that we are the middle of July.
Thank you.

And I can also confirm that CW 6.0 has been available for some time already.

Alban.
0 项奖励
回复

7,209 次查看
HansenOnDk
Contributor I
Haven't told I develop on HCS12.
But I will try again to find some Vista-compatibel CW for this family.
Tadek 
0 项奖励
回复

7,209 次查看
CrasyCat
Specialist III
Hello
 
CodeWarrior for HC12 V4.6, which is the current HC12 release does not support Windows Vista.
This should be supported in a later release of the tools.
 
I do not have a schedule for that one yet.
 
 
CrasyCat
0 项奖励
回复

7,209 次查看
Alban
Senior Contributor II
Oh, that's a bad news :smileysad:

Thank you for the info though, it means I should keep my current workstation !

Alban.
0 项奖励
回复

7,209 次查看
CrasyCat
Specialist III
OK I get an update on Vista support for HC12.
 
CodeWarrior for HC(S)12(X) V5.0 will support Windows Vista.
This release is planned for November 2007.
 
CrasyCat
0 项奖励
回复

7,209 次查看
fabiantp
Contributor I
ey! What happended with CWHC(12) 5.0?? I'm working with the 4.6 on a Virtual Machine.. but it's slowly... Does even a patch been released?
0 项奖励
回复

7,209 次查看
CrasyCat
Specialist III
Hello
 
CodeWarrior for HC12 V5.0 will be delayed.
I did not get an official release date yet.
 
CrasyCat
0 项奖励
回复

7,209 次查看
Jay
Contributor I
Any news on that HC12 V5.0 release?  Having problems with 4.6 on Vista...
 
-Jay
0 项奖励
回复

7,209 次查看
CrasyCat
Specialist III
Hello
 
Just a quick Update on this one.
 
CodeWarrior for HC12 V4.7 is available for download from our Web Site.
 
This release supports Windows Vista OS.
 
To download this release:
     - Click on the link "HCS12(X) Microcontrollers"
     - Click on the "Downloads" tab
     - Now you can decide whether you want to download a Special edition or an evaluation
        version of the software.
 
CrasyCat
0 项奖励
回复

7,209 次查看
Jay
Contributor I
Hi,
 
the 4.7 release seems to be working well now on my Vista laptop.  I can now reliably start debugging using the P&E BDM from within the IDE.
 
Cheers and Thanks!
 
-Jay
0 项奖励
回复

7,209 次查看
geko11
Contributor I
Hi,
i just tried multiple times to install 4.7 on my vista ultimate sp1 and when it is nearing the end of the install wizard, it will stop suddenly and say that:

"The wizard was interrupted before CodeWarrior development studio for hcs12(x) v4.7 could be completely installed."

has any one else had this problem?
what do i do i have been trying for a good two hours to make it work.

thanks


0 项奖励
回复

7,209 次查看
Dome
Contributor II
Hi,

I have the Window Vista Ultimate 64-bit and I have the same problem of Geko11.

What is the problem??
Thanks
0 项奖励
回复

7,209 次查看
trav
Contributor III
Make sure you have version 4.7.  If you do and it still will not install try uninstalling GrooveMonitor which is part of Microsoft Office 2007.  This worked for me.
0 项奖励
回复

7,209 次查看
Dome
Contributor II
Hi,

I try to install "CWHCS12X_v4.7_Eval.exe".
I haven't installed Microsoft Office.

Are there any other tips??
Thanks


0 项奖励
回复

7,209 次查看
trav
Contributor III
Try the special edition.

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600610BF1

It's limited by code size to 32KB which should be enough to evaluate it. 

can also try to download 4.7.1 here

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X&nodeId=0127262E70334A&fpsp=...

0 项奖励
回复

7,209 次查看
Haz
Contributor I
I get the same error about the wizard being interrupted.
Digging a little deeper, I found that it is due to the Vista 64-bit. I am running Vista Ultimate 64-bit. the same install package runs on all 32bit versions, but not the 64. On the IDE webpage, it clearly states that only 32bit versions of windows are supported.
 
Anyone has any idea when Freescale will launch the 64-bit vista support update?
 
Thanks
0 项奖励
回复

7,209 次查看
Metallicajosh
Contributor I
I'm attempting to get some info regarding support for 64bit, hopefully get back soon.
0 项奖励
回复