What is Viinstr Interrupt?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is Viinstr Interrupt?

1,701 Views
ignisuti
Contributor IV

I'm seeing interrupt Viinstr trigger, but I'm not sure why. Can someone please tell me about this interrupt?

 

Also, Where can I get a detailed list telling me about all the available interrupts?

 

MVU: MCF51CN128

IDE: CW 10.1

Labels (1)
0 Kudos
Reply
3 Replies

1,572 Views
J2MEJediMaster
Specialist I

For information on the MCF51CN128RM's interrupt vector table, download the CPU's reference manual from here. Table 5-1 of this document shows the interrupt vector table for the MCF51CN128 series parts.

 

---Tom

0 Kudos
Reply

1,572 Views
ignisuti
Contributor IV

Thanks for the link.

Unfortunatly, I was unable to find "Viinstr" anywhere in that document. 

0 Kudos
Reply

1,572 Views
CrasyCat
Specialist III

Hello

 

According to file mcf51cn128.h,  Viinstr is associated with vector number 4 (#define VectorNumber_Viinstr 4U).

 

According to the table 5-3. ColdFire Exception Vector Table MCF51CN128 reference manual J2MEJediMaster was referencing earlier the exception associated with vector number 4 is Illegal instruction.

 

So you are chaining an Illegal instruction exception here.

 

CrasyCat

0 Kudos
Reply