USB-TAP connectivity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB-TAP connectivity

2,922 Views
bob_s
Contributor III

I would like to be able to connect my USB-TAP to an already running system without having to download code to it.  The Debug options "Attach to process" and "Connect" look like possibilities, but don't work.  There is some documentation on "High Speed Simultaneous Transfer" in my pdf file "Targeting_56800E" page 113 under Host-Side Client Interface that makes me think this should be doable.

 

Bob

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,638 Views
J2MEJediMaster
Specialist I

The Connect choice (Debug > Connect) ought to work, but all you will be able to do is view registers and memory. No symbolic information will be available. See page 186 of the Targeting_56800E Manual.

 

---Tom

0 Kudos
Reply

1,638 Views
bob_s
Contributor III
Thanks, I will look into that function.
0 Kudos
Reply