Is anyone else have problems trying to use Debug when using the P&E USB Multilink and a HCS12 device?
One of the problems seems to be associated with the loading the cmd files.
Example from the Command display:
Loading Target ...
Initializing STARTUP command file:
CMDFILE STARTUP ON "startup.cmd"
Startup Command File execution: startup.cmd
File does not exist: startup.cmd
Startup command file does not exist.
Many thanks
Hello John,
Does the P&E hardware is detected by operating system within device manager ?
If not , please refer to this link to install the drivers :
Hope it helps
Alice