Reconstructing Frac16 Values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reconstructing Frac16 Values

4,112 Views
Law
Contributor I

Gday,

 

I'm a bit new to the Freescale embedded world. I have a 56F8037 Dev board that I have been playing around with for a while now. Well, I am trying to get some serial data out of my board. (I havent been using Freemaster as part of my messings about include a linux host that talks to the board). Anywho, I have serial all up and going, but my problem is during the breaking down of Frac16 values for transmission and reconstruction at the other end.

In essence, I simply want to push out some Frac16 variables over serial so I can view them on my linux host.

 

On the DSC side of things, I have two defines, they are:

 

#define BYTE_L(x) ((x) & (unsigned short)0xFF)

#define BYTE_H(x) ((x >> 8) & (unsigned short)0xFF)

 

I then deconstruct a frac16 and send it over serial using the above defines, IE

sendser(BYTE_H(frac16Val));

sendser(BYTE_L(frac16Val));

 

On the PC side of things, I load the recieved data into a buffer then attempt to reconstruct it. I think this is where the problems arise!

 

I have a function on the PC side that I put the values from the buffer through to reconstruct them in to floating point versions of the Frac16. In theory, the floats should then contain some value from -1 to 0.9999999

 

float build_float(char upper, char lower)
{
    float float_val;
    return float_val = ((float)((((char)upper) << 8) | (char)lower) / 32768);   
}

 

Ie Resultant_Float = build_float(ser_buffer[0], ser_buffer[1]);

 

But, I am not getting expected values back.

 

Could anyone please cast an eye over this and let me know if I am on the right track?

 

Thanks very much,

 

Laurence

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,857 Views
Law
Contributor I

Hi again,

 

I would just like to post a follow up to this.

I was messing around and created 2 programs that sent static info from the DSC to my PC.

 

All it does is send -1 to 1 in increments of 0.1 to the PC, which attempts to reinterpret

 

This is the output:

[ -1.000000 ]
[ -0.001556 ]
[ -0.003113 ]
[ -0.699982 ]
[ -0.599976 ]
[ -0.500000 ]
[ -0.001556 ]
[ -0.003113 ]
[ -0.199982 ]
[ -0.099976 ]
[ 0.000000 ]
[ -0.001587 ]
[ -0.003143 ]
[ 0.299988 ]
[ 0.399994 ]
[ 0.500000 ]
[ -0.001587 ]
[ -0.003143 ]
[ 0.799988 ]
[ 0.899994 ]
[ -0.000031 ]

 

I can see that it is correctly converting some of the values, IE -1, -.7, -.6, -,5 etc, but you can see it just screws up on some of the values!

Any ideas?

0 Kudos
Reply

2,857 Views
ipa
Contributor III

Hi,

You must take into account the endianess of two different micros:

on PC is little endian, so you must send in order sender(BYTE_LSB), sender(BYTE_MSB).

Or take into account that on PC side and re-assemble correctly the word.

Regards,

IPA

0 Kudos
Reply

2,857 Views
Law
Contributor I

Hi there Ipa,

 

Well, I must apologise! I figured this little tidbit out the morning after I posted my last message. So, I'm happy to say, I have it all working. I just neglected to post about it!

 

Thanks again,

 

Laurence

0 Kudos
Reply