Problem with QuickStart tool r2.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with QuickStart tool r2.3

1,866 次查看
z3Lxru
Contributor I

Hi all ,

 

       I'm a beginner using codewarrior 8.2 & I m working with 56F8XXX DSCs. I have problem with quick start tool. I have installed quick start & I have done all the required settings (in prefernces & key bindings). But when I start creating new project I'm not getting the DSP56800E Quick start r2.3 stationery option which I should get. 

 

 I have attached the picture also that shows what I should get.

 

Has any one encountered similiar problem or does any one know the solution for this.

 

Thanks..

Saran

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,010 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

 

I installed the DSP56800EQUICKSTARTSW.exe on my CodeWarrior for DSC56800E v8.2.3 installation.

On my side the DSP56800E_Quick_Start r2.3 project in the File ¦ New is available.

This is defined during the quickstart installation. You must select the CodeWarrior Installation.

 

The project wizard is defined in the \Stationery folder.

After to have installed quickstart, the DSP56800E_Quick_Start r2.3 under the \Stationery.

If it's not the case, you can:

 - re install Quickstart and select the right CodeWarrior installation,

 - move it manually.

 

I recommend you the first solution.

 

Regards

Pascal

0 项奖励
回复