Please help  MC56f8300DSK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Please help  MC56f8300DSK

2,779件の閲覧回数
AuxiliaresFUSM
Contributor I
Hi, I have this problem whit me CodeWarrior. Please Help me.
I have the Kit of the MC56f8300DSK. I download the license but she does not work to me.
 
 
Error   : Unable to use the plugin "Metrowerks M56800E C Compiler". It is licensed and a valid license key was not found.
No such feature exists
Feature:       Win32_Plugins_DSP56800_Full
License path:  C:\Archivos de programa\Metrowerks\CodeWarrior\license.dat
FLEXlm error:  -5,357
For further information, refer to the FLEXlm End User Manual,
available at "www.macrovision.com".
Error   : Unable to use the plugin "Metrowerks M56800E C Compiler". It is licensed and a valid license key was not found.
No such feature exists
Feature:       Win32_Plugins_DSP56800_Full
License path:  C:\Archivos de programa\Metrowerks\CodeWarrior\license.dat
FLEXlm error:  -5,357
For further information, refer to the FLEXlm End User Manual,
available at "www.macrovision.com".
Error   : Unable to use the plugin "Metrowerks M56800E C Compiler". It is licensed and a valid license key was not found.
No such feature exists
Feature:       Win32_Plugins_DSP56800_Full
License path:  C:\Archivos de programa\Metrowerks\CodeWarrior\license.dat
FLEXlm error:  -5,357
For further information, refer to the FLEXlm End User Manual,
available at "www.macrovision.com".
Error   : Unable to use the plugin "M56800E Assembler". It is licensed and a valid license key was not found.
No such feature exists
Feature:       Win32_Plugins_DSP56800_Full
License path:  C:\Archivos de programa\Metrowerks\CodeWarrior\license.dat
FLEXlm error:  -5,357
For further information, refer to the FLEXlm End User Manual,
available at "www.macrovision.com".
Error   : Unable to use the plugin "M56800E Assembler". It is licensed and a valid license key was not found.
No such feature exists
Feature:       Win32_Plugins_DSP56800_Full
License path:  C:\Archivos de programa\Metrowerks\CodeWarrior\license.dat
FLEXlm error:  -5,357
For further information, refer to the FLEXlm End User Manual,
available at "www.macrovision.com".
Error   : Unable to use the plugin "M56800E Assembler". It is licensed and a valid license key was not found.
No such feature exists
Feature:       Win32_Plugins_DSP56800_Full
License path:  C:\Archivos de programa\Metrowerks\CodeWarrior\license.dat
FLEXlm error:  -5,357
For further information, refer to the FLEXlm End User Manual,
available at "www.macrovision.com".
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

909件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hello,
 
I don't know the version you're using.
You can download the DSC 8.0 on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600612247
There is a patch for the DSC8.0 (must be installed in first) DSC8.1.1
You can download it on our web site via the link:
 http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882140B
The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.
For more details about the tool, please have a look to:
 
Regards
Pascal
0 件の賞賛
返信