Open/New file dialog err

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Open/New file dialog err

2,391件の閲覧回数
VrAlex
Contributor I
         Hello, 
         I'm experiencing something very strange when I try to Open or create a New Project in CW 6.1. The IDE will crash/dump when trying to access (read/write) one of the following files: IDE_MFC60cw.dll or IDENewDialog.dll. This will not happen when I open the environment directly by accessing a  *. mcp  file.(or any existing file in a format supported by the IDE).
         I'm 100% sure that the problem is caused by dll read/write privileges but I wasn't able to solve it. I mention that I have full permission over these files but I still get this IDE crush.
         In order to get a full understanding of my problem I attached the .dump file generated by the IDE.
         If you have any suggestions on how can I solve this, please respond as I have run out of ideas.
         Thanks.
 
P.S: I saved the .dump file as a normal txt in order to be able to attach it. 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

951件の閲覧回数
CrasyCat
Specialist III
Hello
 
There is a known incompatibility between CodeWarrior and Office Groove.
 
 Please have a look for FAQ-27815 or FAQ-27460 for possible solutions to fix the issue.
 
CrasyCat
0 件の賞賛
返信