Must convert CodeWarrior IDE .mcp to .mak file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Must convert CodeWarrior IDE .mcp to .mak file

3,476件の閲覧回数
tooldeveloper
Contributor I
I'm developing applications to automate builds and require a way to generate .mak files from the .mcp files that developers are creating and modifying. Is there a way to generate .mak files from .mcp files.
 
This is not for reverse engineering, but rather for automation. Most engineers like the Windows GUI, but for automation and releases we compile from Solaris command line and thus require .mak files - unless the Solaris compiler can actually take the .mcp files which could be another solution.
ラベル(1)
0 件の賞賛
返信
1 返信

1,081件の閲覧回数
CrasyCat
Specialist III
Hello
 Not sure which processor you are targeting.
 Basically today it is not possible to export a .mcp file into a .mak file.
CrasyCat
0 件の賞賛
返信